AC2000 v12 0 Workstation Installation Video

This Video Shows AC2000 v12 0 Workstation Installation Video Time Stamps;00:00 Intro00:10 Prerequisites00:20 Running the Workstation ISO00:35 AC2000 Version01:00 AC2000 Installation Wizard01:55 AC2000 Authentication03:20 Downloading Connection Certificate03:55 Restarting the Workstation04:15 Verifying Install04:49 Outro

AC2000 v12 0 HID Omnikey v5427 Picopass Validation reader Deployment

This Video Shows AC2000 v12 0 HID Omnikey v5427 Picopass Validation reader Deployment Time Stamps:00:00 Intro00:10 Prerequisites00:20 Step 100:18 Checking Drivers Installed02:00 Step 203:00 Step 304:30 Step 405:40 New Features06:55 Using PicoCard Check07:40 Using PicoCard Query08:18 Outro

Pin as Card Function

This Video Shows Pin as Card Function Time Stamps:00:00 Intro00:10 Note00:30 Prerequisites00:40 Step 102:25 Step 203:30 Step 305:50 Step 408:25 Step 510:20 Demo Of how to use Pin on a s700

Setting the DCM400’s IP Address

This Video Shows Setting the DCM400’s IP Address Time Stamps;00:00 Intro00:10 LCD Menu00:20 Navigate to Settings00:30 Navigate to Device Ip Address00:40 Input you DCM’s IP address00:55 Confirming Changed01:15 Outro

Adding an IOC Input Output Controller to the AC2000 Devices Application

This Video shows Adding an IOC Input Output Controller to the AC2000 Devices Application Time Stamps;00:00 Intro00:10 Prerequisites00:25 Logging into AC2000 Floatbar00:40 Navigating to Devices00:55 Navigate to Add MDC01:10 Adding the ADC02:30 Alternatively Adding Input Group To Specific Device Group05:00 Outro